cancel
Showing results for 
Search instead for 
Did you mean: 

About touchGFX.. I installed the touchGFX not under ProgramFiles. When I cuild for target i Get a make error Can someone help solve this ? Thanks Eli

ECrom.2
Associate II
 
5 REPLIES 5
MM..1
Chief III

Normal place of instal isnt in ProgramFiles then your isuue must be other type. Try show error...

ECrom.2
Associate II

But I I installed in another place due to some reasons.

The Build tries to build under Programs files and generates and an error the the files are not there..

MM..1
Chief III

show error

Osman SOYKURT
ST Employee

Hello ECrom.2,

TouchGFX Designer could be installed anywhere on your computer. HOWEVER you must install STM32CubeProgrammer to the default path which is "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer" because this is where TouchGFX Designer will look for when you run on target.

/Osman

Osman SOYKURT
ST Software Developer | TouchGFX
ECrom.2
Associate II

Thanks

There should be a configuration param for this

Eli