2022-06-13 9:56 PM
Hello,
We are working on interface of OV6946 camera with STM32F7508 development kit. We need to capture image and stream on STM32F7508 Display. Camera which we are using provides 10bit output with 400x400 resolution in Bayer’s format.
The connections are done as mentioned below:
Camera Pin Controller Pins
DCMI_D0 - PH9
DCMI_D1 - PH10
DCMI_D2 - PH11
DCMI_D3 - PH12
DCMI_D4 - PH14
DCMI_D5 - PD3
DCMI_D6 - PE5
DCMI_D7 - PE6
DCMI_D8 - PI1
DCMI_D9 - PI2
DCMI_PIXCLK - PA6
DCMI_HSYNC - PA4
DCMI_VSYNC - PG9
DCMI_SDA - PB9
DCMI_SCL - PB8
We are using example code from STM32 Cube example project named “Camera�?.
We are getting black and white scrolling image for the configuration given below
static void LCD_LL_ConvertLineToARGB8888(void *pSrc, void *pDst)
{
/* Enable DMA2D clock */
__HAL_RCC_DMA2D_CLK_ENABLE();
/* Configure the DMA2D Mode, Color Mode and output offset */
hdma2d_eval.Init.Mode = DMA2D_M2M_PFC;
hdma2d_eval.Init.ColorMode = DMA2D_OUTPUT_ARGB8888;
hdma2d_eval.Init.OutputOffset = 0;
/* Foreground Configuration */
hdma2d_eval.LayerCfg[1].AlphaMode = DMA2D_NO_MODIF_ALPHA;
hdma2d_eval.LayerCfg[1].InputAlpha = 0x00;
hdma2d_eval.LayerCfg[1].InputColorMode = DMA2D_INPUT_RGB888;
hdma2d_eval.LayerCfg[1].InputOffset = 0;
hdma2d_eval.Instance = DMA2D;
/* DMA2D Initialization */
if(HAL_DMA2D_Init(&hdma2d_eval) == HAL_OK)
{
if(HAL_DMA2D_ConfigLayer(&hdma2d_eval, 1) == HAL_OK)
{
if (HAL_DMA2D_Start(&hdma2d_eval, (uint32_t)pSrc, (uint32_t)pDst, 200, 1) == HAL_OK)
{
/* Polling For DMA transfer */
HAL_DMA2D_PollForTransfer(&hdma2d_eval, 100);
}
}
}
else
{
/* FatFs Initialization Error */
while(1);
}
}Please refer the link below for output reference:
https://drive.google.com/file/d/1ATyK06csLdJNzLO_H6x2dtP0buMR2cGr/view?usp=sharing
Please guide us, what are the built in configurations are need to be used for converting 10bit Bayer image input to RGB LCD output.
Thanks & Regards,
Ayaz Ahmed,
Riosh Technologies,
Bangalore.
2022-07-20 2:04 AM
Hi @NS.9 ,
When you refer to the RM0385 section 9.3.4 Table 35, you can conclude that the DMA2D can't support the Raw Bayer format input. So, you can't do the conversion from Raw Bayer format to RGB format.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-07-20 2:45 AM
@KDJEM.1 "So, you can't do the conversion from Raw Bayer format to RGB format"
Or, rather, you'll have to do it in software.