cancel
Showing results for 
Search instead for 
Did you mean: 

我在使用STM32CUBEMX生�?GUI代�?完�?�?�,在工程目录TouchGFX里�?�打开Applacation Template.touchgfx.part文件�?�,desigener报错,Error: 无法对 null 引用执行�?行时绑定,请问下这个问题怎么解决

Jzhan.81
Associate III

0693W00000BbjtdQAB.png

12 REPLIES 12
Alexandre RENOUX
Principal

Hello Jzhan.8,

Could you tell us in English the steps you did to arrive to this unexpected error ? Can you reproduce it ?

/Alexandre

Jzhan.81
Associate III

OK,After using stm32cubemx to generate GUI code, I open the application template.touchgfx.part file in the project directory TouchGFX, and the designer reports an error. Error: I can't perform runtime binding on null reference. How can I solve this problem?Thanks~

Jzhan.81
Associate III

Yes,I can reproduce it,it always does that,I haven't sloved it yet.

Jzhan.81
Associate III

When I used STM32CUBEMX to generate GUI code,it's not appearing any warning and wrong.

Alexandre RENOUX
Principal

Hi Jzhan.8,

Could you enclose your .touchgfx.part (and .touchgfx files if you have it) ?

/Alexandre

Jzhan.81
Associate III

Can I add your Wechat or QQ?I can send it to you through it.

Unfortunately I don't have WeChat nor QQ.

You can send it to me by private message on this community.

/Alexandre

Jzhan.81
Associate III

I haved sent it to you through privacy communication.

Your touchgfx.part is empty. It should not happen.

Can you tell me exactly the steps you did to generate it ?

Did you use CubeMX, add the TouchGFX Generator additional software to your project and generate code ?

/Alexandre