TeraTerm not showing printouts
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-18 4:35 PM
I have asked this on ST Online Support. I think I should ask it here too.
I use System Workbench to 'build all' 2 big packages "as is":
- STM32Cube_FW_H7_V1.5.0/Projects/STM32H743I-EVAL/Applications
- STM32CubeExpansion_SBSFU_V2.2.0/Projects/NUCLEO-H753ZI/Application
For demos that use a HyperTerminal (I use TeraTerm), I don't see the debug printouts to terminal. The TeraTerm setup is pretty straightforward:
- Connect STM32H753 target with the PC via USB, a STMicroelectronics STLink Virtual COM Port (COMx) (CN23)
- Open terminal application and connect it via COMx with the following settings: 115200-8-N-1
Is there a switch/jumper on the STM32H753xi EVAL2 Board that I need to change to make this work? I am testing with the following applications:
- STM32Cube_FW_H7_V1.5.0/Projects/STM32H743I-EVAL/Applications/IAP/IAP_Main (use Serial_PutString())
- STM32CubeExpansion_SBSFU_V2.2.0/Projects/NUCLEO-H753ZI/Applications/1_Image (use printf())
The apps are supposed to print/display a menu on TeraTerm for user interactions.
When I unplug/plug the USB, my PC pops up the file explorer showing 'EVA_H753Xi (D:)' drive that has a file called DETAILS.TXT which contains the following lines:
Version: 0221
Build: Jan 11 2019 17:19:2
Solved! Go to Solution.
- Labels:
-
STM32H7 Series
-
X-Cube-SBSFU
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-18 4:49 PM
>> STM32H753xi EVAL2 Board that I need to change to make this work?
Aren't there a pair of jumper that allow you to select between RS232 port or ST-LINK VCP, try checking those.
Code for NUCLEO probably not going to be using same USART and pins as the EVAL2
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-18 4:49 PM
>> STM32H753xi EVAL2 Board that I need to change to make this work?
Aren't there a pair of jumper that allow you to select between RS232 port or ST-LINK VCP, try checking those.
Code for NUCLEO probably not going to be using same USART and pins as the EVAL2
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-18 5:34 PM
Got it. Thank you Clive. I need to configure JP7 and JP8. I will make sure the settings work on STM32H743I-EVAL first before porting the NUCLEO-H753ZI code. I am actually want to use the ST-LINK interface for hyperterminal purpose.