cancel
Showing results for 
Search instead for 
Did you mean: 

stm32F769I IAP

Aravind1
Associate II

Hi,

I am trying to implement IAP through UART on stm32f779I Evaluation kit,  I am using stm cude IDE 1.9.0 and F7v1.17.0 software package.

I have downloaded IAP_Main project using st_link. By using tampered button entered into the downlaod mode and using teraterm tried to load the binary file of IAP_SingleBinary_Template example code from the examples through YModem protocol. My IAP is working fine but when it comes to downloading the binary file teraterm is showing only 2 packets is loaded and the file transfer window is getting disappear.

Can anyone please help me to find out the issue.

 

Thanks & Regards,

k. Aravind

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Not sure of the robustness of the Y-MODEM implementation. You're probably going to need to do some bus analysis on the serial port traffic, and/or add some SWV based telemetry to the STM32 side code so you can understand specifically what's happening. 

Familiarity with the protocol would help. Perhaps try other implementations, or your own.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..