2024-07-22 03:03 AM - edited 2024-07-22 07:48 AM
Hi,
{EDIT 2] : I fixed few typo, and also fixed my explanation : I made few confusion when reporting my notes ==> both DMA channel 10 source and destination are secure, with source == ADC1 channel 10 and destination (via linked list) is a buffer in SRAM3.
A bit of context: I have to start ADC conversion on 3 channels, with ADC1, and it must be done in Secure world.
To do things step by step I first started with no TrustZone activated, and from STM32CubeMX I successfully generated code to use ADC1 on 3 channels, with DMA in linked list mode, without Trust Zone activated.
Note: the code generated by MX does not include anything to "link" the ADC1 with the DMA linked list, so I had to take the code from the example available "ADC DMA transfer" in MCU package. It means I had to add this piece of code in the main function of the project:
/* USER CODE BEGIN 2 */
MX_ADCQueue_Config();
__HAL_LINKDMA(&hadc1, DMA_Handle, handle_GPDMA1_Channel10);
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel10, &ADCQueue) != HAL_OK)
{
Error_Handler();
}
if (HAL_ADC_Start_DMA(&hadc1,
(uint32_t *)aADCxConvertedData,
(ADC_CONVERTED_DATA_BUFFER_SIZE)
) != HAL_OK)
/* USER CODE END 2 */
(and I had to add the C files "linked_list.c" from the example of MCU package).
All of this work fine without TrustZone : I can put break point in the Channel10 IRQ handler and see I regularly enter it and the buffer provided to the DMA linked list is filled with data from channel 0, 1 and 2 as expected.
This is really nice, so I started a new MX project, this time with TrustZone activated. I set ADC1 to Secure, configure it the same way as above (aka 3 channels etc.), configured DMA channel 10 to be secure/non privileged, circular mode etc. That is I configured the same behaviour as without TrustZone.
I generate code, for IAR ide. Here again, the code to glue ADC and DMA linked list is not generated (I think I should create a 2nd post for this issue, this will be done later), so I add it manually.
Since the SRAM3 is secured, I configure my DMA channel this way:
- non privileged (done by generated code)
- secure (done by generated code)
- source is secured : this is not done by MX, I have to do it manually
- destination is secured : this is not done by MX, I have to do it manually
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel10, DMA_CHANNEL_NPRIV|DMA_CHANNEL_SEC|DMA_CHANNEL_SRC_SEC|DMA_CHANNEL_DEST_SEC) != HAL_OK)
{
Error_Handler();
}
All in all it looks fine, I build and run : and of course it does not work :D : I enter only one time the DMA IRQ handler, the method "HAL_DMA_IRQHandler" is detecting an error "User Setting Error Interrupt management" (this is the comment in C code. But if you go to headers you will read "User Setting Error Interrupt enable"). And the buffer I expect to see filled with data from ADC is not updated at all : it's full of 0.
i tried various investigation, and found:
ERRATA: the call to __HAL_RCC_GTZC1_CLK_ENABLE() is actually done in HAL_MspInit from file stm32u5xx_hal_msp.c.
- I notice __HAL_RCC_GTZC1_CLK_ENABLE() is not called in generated code MX_GTZC_S_Init : I add it but it makes no difference
- I notice GPIOC port 0, 1 and 2 for channels are not configured as secure (maybe I did not find where ?). So I added in generated code "HAL_ADC_MspInit", but it changes nothing. :
HAL_GPIO_ConfigPinAttributes(GPIOC, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2, GPIO_PIN_SEC);
- Found that when using DMA linked list, there is also something to configure for source and destination related to security, so I added this, but it changes nothing
DMA_NodeConfTypeDef pNodeConfig;
...
...
pNodeConfig.SrcSecure = DMA_CHANNEL_SRC_SEC;
pNodeConfig.DestSecure = DMA_CHANNEL_DEST_SEC;
...
...
ADC1 is set to Secure and non privileged:
if (HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_ADC12, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV) != HAL_OK)
Vdda is enabled.
It do not know what to look with this USEF flag, what it means.
Well, right now I do not know how/where to investigate this problem. I'm pretty sure it(s obviously right under my eyes, but I need help here. Maybe everything that should be done is done but not in the correct order ?
Is there anyone with some idea ?
Many thank in advance to you.
P.