2017-03-30 1:13 AM
Hi,
I would like to use a software read protection on STM32F0. I've made such a function:
PROTECT_STATUS ReadProtectionConfig(uint8_t ProtectionLevel)
{ uint8_t status = OK; FLASH_OBProgramInitTypeDef OB_Init; HAL_FLASH_Unlock(); HAL_FLASH_OB_Unlock(); OB_Init.OptionType = OPTIONBYTE_RDP; if (ProtectionLevel == 0) { OB_Init.RDPLevel = OB_RDP_LEVEL_0; } else if (ProtectionLevel == 1) { OB_Init.RDPLevel = OB_RDP_LEVEL_1; } else if (ProtectionLevel == 2) { OB_Init.RDPLevel = OB_RDP_LEVEL_2; } else { status = RDPLevel_Error; return status; }HAL_FLASHEx_OBProgram(&OB_Init);
HAL_FLASH_OB_Launch(); HAL_FLASH_OB_Lock(); HAL_FLASH_Lock(); return status;}but it don't work properly. I mean even if I choose
OB_RDP_LEVEL_0 it blocks read out of flash memory. It is because the program can't perform the HAL_FLASH_OB_Launch(); function.
My problem is that I don't know why it happens and what should I do to make it better.
Could you help me?
Regards,
Kasia
#stm32f0-read-out-protection #read-out-protection #stm32f072 #stm32f02017-03-30 9:35 AM
Hi
Bartnik.Katarzyna
Please try to start from ready example under the STM32F0 cube firmware package:
STM32Cube_FW_F0_V1.7.0\Projects\STM32091C_EVAL\Examples\FLASH\FLASH_WriteProtection
-Nesrine-
2017-04-03 1:54 AM
Hi Nesrine M,
This example doesn't pertain to my problem, because it is write protection. I know that it is very similar. I think that a scheme of my program is the same like in the example, but it doesn't work properly.
Regards
Kasia
2018-05-14 11:25 PM
Hello Kasia,
I have prepared a simple application using your function. Key point here is to take care to execute protection function only once, thus in my example I am using one of the backup registers which are reset only on power on reset. Just before set protection (even to level0) I am writing there 0xA5A5, then on OB reload when the MCU is reseted I check whether I have not done already modification of the protection and if yes, I am skipping this process. Otherwise I would set protection to level0 continuously.
In main loop I am toggling PC6 pin.
Whole application I have tested on STM#2F072B-Discovery using Atollic True Studio 9.0.1.
I am attaching you main.c file and my .ioc project file for STM32CubeMX.
Could you please test it on your side?
Best Regards,
Artur
________________ Attachments : RDP0.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxXe&d=%2Fa%2F0X0000000b0K%2F0MyA7zBVeGWe.gcH0iosirOZ3gNnNgHiCDrfyInUu3o&asPdf=falsemain.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxd7&d=%2Fa%2F0X0000000b0I%2Fl.Q3yLEYU4ljiWBtp6A8x4aM8fobMvRx3E2_WZ7Zln0&asPdf=false