STM32 cryptografic AES CCM libraries giving wrong results
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-06-30 8:40 AM
Hello everyone
I am trying to use the crypto library to perform an AES CCM encryption decryption. I am using an STM32F423CH MCU. The frames I am receiving are comming from other system and the authentication is always failing.
I implemted the validation scheme that appears in the NIST Special Publication 800-38C for CCM.
//FROM THE EXAMPLE IN nvlpubs.nist.gov
const uint8_t key[] = {0x40, 0x41, 0x42, 0x43, 0x44, 0x45, 0x46, 0x47, 0x48, 0x49, 0x4A, 0x4B, 0x4C, 0x4D, 0x4E, 0x4F};
uint8_t nonce[] = {0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16};
uint8_t header[] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07};
uint8_t data[] = {0x20, 0x21, 0x22, 0x23};
uint8_t outputData[40];
uint8_t outputTag[8];
uint8_t recoveredData[32];
int32_t outputLength = 4;
int32_t outputTagLength;
volatile uint32_t error_status = AES_SUCCESS;
AESCCMctx_stt AESCCMctx;
AESCCMctx_stt* AESctx = &AESCCMctx;
AESctx->mNonceSize = 7;
AESctx->mKeySize = CRL_AES128_KEY;
AESctx->mFlags = E_SK_DEFAULT;
AESctx->mAssDataSize = 8;
AESctx->mTagSize = 4;
AESctx->mPayloadSize = 4;
AESctx->pmTag = outputTag;
error_status = AES_CCM_Encrypt_Init(AESctx, key, nonce);
error_status = AES_CCM_Header_Append(AESctx, header, 8);
error_status = AES_CCM_Encrypt_Append(AESctx, data, 4, outputData, &outputLength);
error_status = AES_CCM_Encrypt_Finish(AESctx, outputData + 4, &outputTagLength);
I am using the SMALL implementation from the library. The expected output is:
MSG:0x71 0x62 0x01 0x5b
MAC: 0x4d 0xac 0x25 0x5d
But the result I am getting is:
MSG: 0x02 0x20 0x1d 0x49
MAC: 0x49 0x37 0x36 0xab
Though the decryption with the same libraries gives a positive result
AESctx->mNonceSize = 7;
AESctx->mKeySize = CRL_AES128_KEY;
AESctx->mFlags = E_SK_DEFAULT;
AESctx->mAssDataSize = 8;
AESctx->mTagSize = 4;
AESctx->mPayloadSize = 4;
AESctx->pmTag = outputData + 4;
error_status = AES_CCM_Decrypt_Init(AESctx, key, nonce);
error_status = AES_CCM_Header_Append(AESctx, header, 8);
error_status = AES_CCM_Decrypt_Append(AESctx, outputData, 4, recoveredData, &outputLength);
error_status = AES_CCM_Decrypt_Finish(AESctx, recoveredData, &outputLength);
Error_status = 1003 (SUCCESS) and the message match with the original.
Am I doing something wrong? Using the mbedtls libraries is working fine.
Thank you in advance for any support.
Solved! Go to Solution.
- Labels:
-
Cryptography
-
STM32F4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-04 2:50 PM
First problem solved! I did not activate the CRC module before using the firmware version of the Cryptographic Library. Thanks to the video "Security Part3 - STM32 Security features - 30 - Crypto library lab"!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-03 5:38 AM
Something is completly wrong somewhere. I have been doing steps in different location and going to the basics but it is still not working.
I activated the AES HW aceleration module to do the encryption/decryption there. I did not get CCM working but going even further I tried to replicate the example on the STM video tutorial on youtube:
Security Part3 - STM32 Security features - 25 - AES CRYPT lab (I cannot add the link directly).
This video tries to replicate one of the examples of the ECB encryption/decryption of the standard NIST Special Publication 800-38A. I am trying to replicate exactly the same example.
The function HAL_CRYP_Encrypt used in this video is not available in the version of the HAL drivers I am using (V.1.21.0) but i tried using the functions HAL_CRYP_AESECB_Encrypt and HAL_CRYPEx_AES. I even tried using the 32bits and the 8 bits configuration posibilities but none of them gave the expected result:
CRYP_HandleTypeDef hcryp;
__ALIGN_BEGIN static const uint8_t pKeyAES[32] __ALIGN_END = {
0x60,0x3D,0xEB,0x10,0x15,0xCA,0x71,0xBE,0x2B,0x73,
0xAE,0xF0,0x85,0x7D,0x77,0x81,0x1F,0x35,0x2C,0x07,
0x3B,0x61,0x08,0xD7,0x2D,0x98,0x10,0xA3,0x09,0x14,
0xDF,0xF4};
CAN_HandleTypeDef hcan1;
SPI_HandleTypeDef hspi1;
TIM_HandleTypeDef htim1;
UART_HandleTypeDef huart1;
DMA_HandleTypeDef hdma_usart1_rx;
DMA_HandleTypeDef hdma_usart1_tx;
osThreadId defaultTaskHandle;
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
__ALIGN_BEGIN static const uint32_t pKeyAES32b[8] __ALIGN_END = {
0x603DEB10,0x15CA71BE,0x2B73AEF0,0x857D7781,0x1F352C07,
0x3B6108D7,0x2D9810A3,0x0914DFF4};
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_TIM1_Init(void);
static void MX_SPI1_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_CAN1_Init(void);
static void MX_AES_Init(void);
void StartDefaultTask(void const * argument);
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
/* USER CODE END PFP */
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
*
* @retval None
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_TIM1_Init();
MX_SPI1_Init();
MX_USART1_UART_Init();
MX_CAN1_Init();
MX_AES_Init();
/* USER CODE BEGIN 2 */
// Plaintext 6bc1bee22e409f96e93d7e117393172a
// Input Block 6bc1bee22e409f96e93d7e117393172a
// Output Block f3eed1bdb5d2a03c064b5a7e3db181f8
// Ciphertext f3eed1bdb5d2a03c064b5a7e3db181f8
uint32_t plaintext32b[4] = {0x6bc1bee2, 0x2e409f96, 0xe93d7e11, 0x7393172a};
uint32_t encryptedData32b[4];
uint32_t decryptedData32b[4];
uint8_t plaintext[16] = {0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96, 0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a};
uint8_t encryptedData[16];
uint8_t decryptedData[16];
volatile HAL_StatusTypeDef ret;
ret = HAL_CRYPEx_AES(&hcryp, (uint8_t*)plaintext32b, 4, (uint8_t*)encryptedData32b, 1000);
if (ret != HAL_OK)
{
while(1);
}
ret = HAL_CRYP_AESECB_Encrypt(&hcryp, (uint8_t*)plaintext32b, 4, (uint8_t*)encryptedData32b, 1000);
if (ret != HAL_OK)
{
while(1);
}
ret = HAL_CRYP_AESECB_Decrypt(&hcryp, (uint8_t*)encryptedData32b, 4, (uint8_t*)decryptedData32b, 1000);
if (ret != HAL_OK)
{
while(1);
}
ret = HAL_CRYP_DeInit(&hcryp);
hcryp.Init.pKey = (uint8_t *)pKeyAES;
if (HAL_CRYP_Init(&hcryp) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
ret = HAL_CRYP_AESECB_Encrypt(&hcryp, plaintext, 16, encryptedData, 1000);
if (ret != HAL_OK)
{
while(1);
}
ret = HAL_CRYP_AESECB_Decrypt(&hcryp, encryptedData, 16, decryptedData, 1000);
if (ret != HAL_OK)
{
while(1);
}
/* USER CODE END 2 */
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* Create the thread(s) */
/* definition and creation of defaultTask */
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
/* USER CODE END RTOS_THREADS */
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
I am starting to think that something it mad in my MCU or in the drivers. Can please someone support!?
Best regards
PS: As commented before using the MBEDTLS SW I got it working straight forward. Regretfully this is too slow for my application. Any advice would be greatly wellcome.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-04 2:50 PM
First problem solved! I did not activate the CRC module before using the firmware version of the Cryptographic Library. Thanks to the video "Security Part3 - STM32 Security features - 30 - Crypto library lab"!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-08 5:33 AM
This is one of the gotchas with the libraries, this needs to be emphasized in the examples and README file.
And honestly a requirement that needs to be removed, and moved beyond.
Up vote any posts that you find helpful, it shows what's working..