Skip to main content
EOCon.1
Associate II
Oct 14, 2021 8:59 AM UTC
Solved

Starting Point advice for STM32L451 Cryptographic Peripheral

Hi all,

I would like to use the Cryptographic peripheral in my STM32L451 to encode and decode some data based on a pre-stored common key.

Are there any examples for Atollic that would get me started on this?

This topic has been closed for replies.
EOCon.1
EOCon.1Best answer
Associate II
Oct 14, 2021 10:13 AM UTC

Problem solved, my L451 does not have the hardware peripheral,only the big brother of this family

3 replies

ST Technical Moderator
Oct 14, 2021 9:16 AM UTC

Hello @Community member​ ,

I adivse you to refer to the HAL example within STM32CubeL4 firmware and you can easily port it on the STM32L451:

STM32Cube_FW_L4_V1.17.0\Projects\STM32L476G-EVAL\Examples\CRYP

You can also download the STM32CubeExpansion_Crypto_V4.0.1 library, and easily port the STM32L4 example according to your needs.

Hope this helps you!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
EOCon.1
EOCon.1Author
Associate II
Oct 14, 2021 9:25 AM UTC

ok, is there a reason why there is zero mention of CRYP or AES in the file the stores all of the register base addresses?

https://raw.githubusercontent.com/STMicroelectronics/cmsis_device_l4/master/Include/stm32l451xx.h

I have tried to look at some example but in the stm32l4xx_hal_cryp.h file there is this definition AES_TypeDef *Instance; /*!< Register base address */

This definition should be defined in my link along with the register layout but it is not, can you please explain why?

Please show me which file has the register map for the AES peripheral.

EOCon.1
EOCon.1AuthorBest answer
Associate II
Oct 14, 2021 10:13 AM UTC

Problem solved, my L451 does not have the hardware peripheral,only the big brother of this family