2024-07-15 5:09 AM
Hello,
The TFM application that is based on the stm32u585 board could work for the stm32u575zit6 microcontroller? I have modified the TFM project and I have removed hw accelerator from the SBSFU project because the u575 microcontroller does not contain this peripheral but in the TFM_Appli application I get cryptographic errors when building the project.
Thanks in advance
2024-07-15 6:30 AM
The STM32U575 doesn't have cryptographic functionality. If the project uses those features, it cannot be ported to that chip.
What errors do you get? Be specific with screenshots if possible.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.