2018-03-11 11:21 PM
Hi
How do i proceed to write a &sharpsecure boot on STM32L4RXX, with out &sharpHW Crypto.
I need to make it by Software later i want to use the HW Crypto provided.
Thanks.,
Phani
#secure-boot2018-03-12 06:10 AM
Hello
phanirajkiran.ma
,I'd highly recommend you to refer to the '
http://www.st.com/en/embedded-software/x-cube-sbsfu.html
' (Secure Boot and Secure Firmware Update solution). It allows the update of the STM32 microcontroller built-in program in a secure way.The software comes with an example implementation running on NUCLEO-L476RG.Do not hesitate to post your questions here if you need further information.
Khouloud.
2018-03-14 08:00 AM
Hello Team,
Last 2 days back i kept request for X-CUBE-SBSFU, still its in validating process.
Please resolve my ticket/ request for software. And send me the link so that i can proceed with SBSFU.
Regards
Phanirajkiran
2018-03-15 02:21 AM
Yes i received.
Thank you.
2018-03-15 03:04 AM
Hi
phanirajkiran.ma
,Have you received the confirmation mail with the link to download the library?
Khouloud.
2018-03-15 03:45 AM
You're welcome and sorry for the delay