2024-06-21 5:18 AM
Hello, I hope you are doing well!
I developed a project based on the STM32H573I-DK example with TrustZone. However, in the final board, I am using the STM32H573VI microcontroller. I migrated all the code to this microcontroller, made the necessary pin ports, and some adjustments. I managed to compile it successfully. Now that the final board is ready, I am trying to run the code, but I am facing an issue with using the provisioning_auto.bat script.
Below are some logs:
Apparently, I am not able to communicate with the hardware using the STLINK-V3PWR through the provisioning_auto.bat script. However, I tested using the STM32CubeProgrammer and was able to connect with the microcontroller.
Can anyone help me? Thanks in advance!
2024-06-24 9:49 AM
Hello @ffjunq ,
the issue is at the end of your log file:
"Error: The file appli_0.hex does not exist, please check the file's path"
This file should be located in ROT_Provisioning/SM/Binary this is the default application.
So, I suspect an issue related to your porting.
Best regards
Jocelyn