possible bug in F3xx Firmware?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-17 1:35 AM
When I compile a simple programm, using the CRC feature I get the following warning:
In file included from ../Drivers/STM32F3xx_HAL_Driver/Inc/stm32f3xx_hal_def.h:30,
from ../Drivers/STM32F3xx_HAL_Driver/Inc/stm32f3xx_hal_rcc.h:29,
from ../Core/Inc/stm32f3xx_hal_conf.h:199,
from ../Drivers/STM32F3xx_HAL_Driver/Inc/stm32f3xx_hal.h:30,
from ../Drivers/STM32F3xx_HAL_Driver/Src/stm32f3xx_hal_crc.c:46:
../Drivers/STM32F3xx_HAL_Driver/Src/stm32f3xx_hal_crc.c: In function 'HAL_CRC_DeInit':
../Drivers/CMSIS/Device/ST/STM32F3xx/Include/stm32f3xx.h:193:41: warning: overflow in conversion from 'int' to 'uint8_t' {aka 'volatile unsigned char'} changes value from '(int)hcrc->Instance->IDR & -256' to '0' [-Woverflow]
193 | #define CLEAR_BIT(REG, BIT) ((REG) &= ~(BIT))
| ^
../Drivers/STM32F3xx_HAL_Driver/Src/stm32f3xx_hal_crc.c:203:3: note: in expansion of macro 'CLEAR_BIT'
203 | CLEAR_BIT(hcrc->Instance->IDR, CRC_IDR_IDR);
| ^~~~~~~~~
Can I ignore that or is that a bug?
Thank you & best regards,
chris
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-17 5:44 AM
Hi @CBerg​ ,
Thank you for rising this up.
I confirm this warning that reproduced with the STM32CubeF3 V1.11.3.
This warning impacts several series and already detected with STM32CubeF0 MCU package:
This issue is already raised internally with ID 133673
(PS: ID 133673 is an internal tracking number and only for reference, not available outside of ST)
The next release of STM32CubeF3 package contains the fix will be published in the coming days.
Hope my answer helped you!
When your question is answered, please close this topic by choosing Select as Best.
Imen
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-17 2:55 AM
Hello @CBerg​
Is this issue reproduced when generated your project with CubeMx ?
Which version of CubeF3 and CubeMX used?
I will check this issue and come back to you soon with update.
Imen
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-17 3:12 AM
I am using STM32CubeIDE 1.10.1 Build: 12716_20220707_0928 (UTC)
It is reproducible. Each time I change something in the .ioc file, let the code generation run and compile it, the warning pops up again
I have no idea, where this comes from, because in
HAL_CRC_DeInit(CRC_HandleTypeDef *hcrc) <stm32fxx_hal_crc.c>
hcrc->Instance->IDR is defined as uint8_t
and in stm32f303x8.h the symbol "CDC_IDR_IDR" is defined as "((uint8_t)0xFFU)"
IMHO both values are uint8_t, no overflow should occur. I have no idea why the compiler asumes, there would be an int involved ...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-17 5:21 AM
Get rid of (uint8_t) typecast in the defined constant. Generally #defines with typecasts are not a good idea, but somehow ST loves them.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-01-17 5:44 AM
Hi @CBerg​ ,
Thank you for rising this up.
I confirm this warning that reproduced with the STM32CubeF3 V1.11.3.
This warning impacts several series and already detected with STM32CubeF0 MCU package:
This issue is already raised internally with ID 133673
(PS: ID 133673 is an internal tracking number and only for reference, not available outside of ST)
The next release of STM32CubeF3 package contains the fix will be published in the coming days.
Hope my answer helped you!
When your question is answered, please close this topic by choosing Select as Best.
Imen
Thanks
Imen