2020-08-11 05:40 AM
I've heard that the next x-cube sbsfu release would include a fix for the ymodem protocol, such that it can be used from linux, and that it would be released by end of July.
Does anybody know when it will be released?
2020-08-25 08:50 AM
Hi @stratom ,
A new release of X-CUBE-SBSFU will be available soon on the web.
However, I am not sure to understand the issue "the ymodem protocol, such that it can be used from linux" to confirm if it is fixed or not.
Could you please provide some more details about this issue?
Thanks,
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-08-31 12:44 AM
Thanks.
According to https://community.st.com/s/question/0D53W00000Eba1XSAR/download-firmware-by-ymodem-failed-at-linux it seems to be the case.