2019-06-12 4:20 AM
I found from this question, on May 2017,
that hardware crypto support was in development for mbedTLS.
When we will get an update with this implemented?
2019-06-12 4:54 AM
You can find the implemented functions under the mbed-os tree's mbedtls "feature":
https://github.com/ARMmbed/mbed-os/tree/master/features/mbedtls/targets/TARGET_STM
2019-06-12 9:29 AM
Thanks for let me know! I was checking it but it was developed by an older HAL driver version (no longer supported) :\ New HAL driver does not have legacy support.
2019-06-14 3:36 AM
HI,
As it was said in this discussion, a ST HW crypto implementation is available on Arm mbed OS but it is done on HAL crypto legacy.
In parallel, F7 came with a HAL (V1.2.7) supporting a new HAL Crypto API because of driver improvement.
How to drive this new HAL crypto API is given in this example : Firmware\Projects\STM32756G_EVAL\Examples\CRYP\CRYP_AESModes
Note most of the code from Arm mbed OS can also be reused. A proposition is given (see attached file) with this new API, as example.
As usual, you must configure Mbed TLS (use MBEDTLS_AES_ALT) and HAL (use HAL_CRYP_MODULE_ENABLED).
Regards.
Thierry
2019-06-17 8:11 AM
Hi Thierry, thanks for the files!
I managed to build it but I had to reduce some of support features as they are not all implemented on this AES,
also, I cannot get it pass the AES tests from mbedTLS, when I run the test file I got:
AES-ECB-128 (dec): passed
AES-ECB-128 (enc): passed
AES-ECB-192 (dec): passed
AES-ECB-192 (enc): passed
AES-ECB-256 (dec): passed
AES-ECB-256 (enc): passed
AES-CBC-128 (dec): passed
AES-CBC-128 (enc): failed
Do you have also the implementation for other features if you can share? md5 and sha256 ?