Hello,I would suggest to test with a Plaintext placed :- in a certain memory boundary (even address divisible by 4).- with a buffer size having extra bytes so that it matches with a multiple of words.Thierry
Hello,BG96MAR02A06M1G is the factory FW cellular modem and must be upgraded.I would suggest to upgrade the BG96 FW modem version with a newest version.For instance, you can find BG96MAR02A07M1G_010 under https://stm32-c2c.com in precompiled Demos Rep...
HI,As it was said in this discussion, a ST HW crypto implementation is available on Arm mbed OS but it is done on HAL crypto legacy.In parallel, F7 came with a HAL (V1.2.7) supporting a new HAL Crypto API because of driver improvement.How to drive th...
Hi,Note that working with a LCD is possible but comsumption may be taken into account, especially when working in parallel with 2G technologies.2G burst may need more power in limit of 2G cellular coverage.A micro B USB cable can optionally be used a...