Use of STM32L4 HAL_CRYP hardware in LORAWAN
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-08 10:51 PM
I've tried to find an example code of use of crypto harware accelerator in LORAWAN but i haven't been able to find any . Does someone have an example expecially concerning the use of AES CMAC?
Regards
- Labels:
-
Cryptography
-
LoRa
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-09 8:12 AM
If you have a chip with the CYPT unit the examples for the EVAL, and other, boards can be ported into other applications and use cases.
STM32Cube_FW_L4_V1.14.0\Projects\STM32L476G-EVAL\Examples\CRYP\CRYP_GCM_GMAC_CMAC_Modes
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
‎2019-06-09 10:31 AM
Thank you, the example is nice for CMAC implementation, regards!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-15 2:33 AM
still strugglign with LORAWAN CMAC... i've made this code, but i'm making a mistake...
// original code modified
void LoRaMacComputeMic( const uint8_t *buffer, uint16_t size, const uint8_t *key, uint32_t address, uint8_t dir, uint32_t sequenceCounter, uint32_t *mic )
{
MicBlockB0[5] = dir;
MicBlockB0[6] = ( address ) & 0xFF;
MicBlockB0[7] = ( address >> 8 ) & 0xFF;
MicBlockB0[8] = ( address >> 16 ) & 0xFF;
MicBlockB0[9] = ( address >> 24 ) & 0xFF;
MicBlockB0[10] = ( sequenceCounter ) & 0xFF;
MicBlockB0[11] = ( sequenceCounter >> 8 ) & 0xFF;
MicBlockB0[12] = ( sequenceCounter >> 16 ) & 0xFF;
MicBlockB0[13] = ( sequenceCounter >> 24 ) & 0xFF;
MicBlockB0[15] = size & 0xFF;
#ifdef USE_HAL_CRYP_MODULE
AES128_CMAC_digest(buffer, size,MicBlockB0, key, Mic);
#else
AES_CMAC_Init( AesCmacCtx );
AES_CMAC_SetKey( AesCmacCtx, key );
AES_CMAC_Update( AesCmacCtx, MicBlockB0, LORAMAC_MIC_BLOCK_B0_SIZE )
AES_CMAC_Update( AesCmacCtx, buffer, size & 0xFF )
AES_CMAC_Final( Mic, AesCmacCtx );
#endif
*mic = ( uint32_t )( ( uint32_t )Mic[3] << 24 | ( uint32_t )Mic[2] << 16 | ( uint32_t )Mic[1] << 8 | ( uint32_t )Mic[0] );
}
//************* then the function using hardware CMAC looks like *****************************
void __attribute__((section(".OSmsk"))) AES128_CMAC_digest(uint8_t* input, uint16_t size, uint8_t* MicBlockB0, const uint8_t* key, uint8_t* output){
hcrypt.Init.DataType = CRYP_DATATYPE_8B ;
hcrypt.Init.KeySize = CRYP_KEYSIZE_128B ;
hcrypt.Init.pKey = key;
hcrypt.Init.OperatingMode = CRYP_ALGOMODE_TAG_GENERATION;
hcrypt.Init.ChainingMode = CRYP_CHAINMODE_AES_CMAC;
hcrypt.Init.GCMCMACPhase = CRYP_GCMCMAC_HEADER_PHASE;
hcrypt.Init.KeyWriteFlag = CRYP_KEY_WRITE_ENABLE;
hcrypt.Init.Header = (uint8_t *)input;
hcrypt.Init.HeaderSize = CMAC_HEADER_SIZE;
/****************************************************************************/
/* De-initialize then initialize the AES peripheral */
/****************************************************************************/
if (HAL_CRYP_DeInit(&hcrypt) != HAL_OK)
{
breakpoint();
}
/* Set the CRYP parameters */
if (HAL_CRYP_Init(&hcrypt) != HAL_OK)
{
breakpoint();
}
/*----------------------------------------------------------------------------------------------*/
/* CMAC header phase */
if (MicBlockB0!=NULL){
if (HAL_CRYPEx_AES_Auth(&hcrypt, (uint8_t *)MicBlockB0, CMAC_B_SIZE, NULL, 100)!= HAL_OK)
{
breakpoint();
}
}
/*----------------------------------------------------------------------------------------------*/
/* CMAC final phase */
hcrypt.Init.GCMCMACPhase = CRYP_GCMCMAC_FINAL_PHASE;
if (HAL_CRYPEx_AES_Auth(&hcrypt, (uint8_t *)input, size, NULL, 100)!= HAL_OK)
{
breakpoint();
}
}
Does anyone made LORAWAN CMAC working using STM32 hardware HAL_CRYP?
Regards