2020-04-07 9:14 AM
I am using STM32F207. The project that im working on will later on will be used by a bootloader. I am, therefore, trying to add crc information in the hex file so that bootloader will be able to validate its correctness.
I am using srec_cat to calculate the crc in postbuild using this example
with a modification that i use obj_copy to fill the memory gaps rather than srec_cat. (--gap-fill 0xFF)
I have added a section in linker file, with the same address as that the one used by srec_cat,
/* Sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
/*placing section for crc */
.crc32 0x08010000:
{
KEEP(*(.crc32)) /*keep my variable even if not referenced*/
} >FLASH
/* The program code and other data into "FLASH" Rom type memory */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
.....and
const uint32_t __attribute__ ((section(".crc32"))) crc_crc32;problems:
Ples help
Solved! Go to Solution.
2020-04-08 5:36 PM
extern uint32_t *g_pfnVectors[];
printf("%p %p\n",g_pfnVectors[0], g_pfnVectors[1]);
2020-04-07 9:55 AM
Who is Ples?
>>since i would have to jump over the memory location on which the crc is, i am using HAL_CRC_calculate along with accumulate, is this the right way of doing it?
Show the code, show an example of the values written in the file vs computed
What's the exact batch file?
The one cited does 0x08000000 thru 0x08007FFB with the CRC at 0x08007FFC, and not 0x08000000..0x0800FFFF, 0x08010000
2020-04-08 5:31 AM
C:\ST\STM32CubeIDE_1.0.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\objcopy.exe --gap-fill 0xFF -O ihex SGW.elf "SGW.hex"
..\srec_cat.exe SGW.hex -Intel -exclude 0x8010000 0x8010004 -STM32 0x08010000 -o SGW_crc.hex -Intel --contradictory-bytes=errorbatch file
Couldn't calculate the crc, as i have no buffer length to pass to HAL_CRC_Accumulate but i think it would be something like this
HAL_CRC_Calculate(&hcrc, (uint32_t*) 0x08000000, (0x08010000 - 0x08000000) / 4;);
crc_cal = HAL_CRC_Accumulate(&hcrc, (uint32_t*) 0x08010004, (firmwareLength - 0x08010004) / 4);and then comparing the result of crc_cal and crc_crc32(see the original question on how i think i would be able to have the value at this variable
2020-04-08 6:18 AM
Also think about another option - introducing 512 byte (because of VTOR alignment requirement) header before the firmware. There you can put CRC, SHA, digital signature, symmetric encryption key (encrypted by asymmetric encryption), product ID, hardware and software version numbers, actual firmware address and other things you need.
As for an actual bootloader design... Do not follow the ST's dumb examples and read my post there:
2020-04-08 9:39 AM
Not sure I understand why you have a hole in the middle to accommodate the CRC.
I would generally let the linker determine the image length, and have it stored in an unused vector in the vector table, and place the CRC at the end.
The nature of the math would be if you run the check over the image and appended CRC, the resultant CRC would be ZERO
linker.ld
...
/* End section */
. = ALIGN(4);
.endof :
{
/* This is used by the startup in order to find the end */
_limit_flash = .; /* define a global symbol at the end of flash */
_flash_size = _limit_flash - g_pfnVectors; /* compute length based on beginning and ending points */
} >FLASH
...
startup.s
...
.word UsageFault_Handler
.word _limit_flash - g_pfnVectors /* compute size */
.word 0
.word 0
...
https://community.st.com/s/question/0D50X00009Xkhp1SAB/flash-crc-integrity
https://community.st.com/s/question/0D50X0000Awa25q/generated-binary-file-size-in-stm32l4
2020-04-08 1:44 PM
i am trying
extern uint32_t __attribute__ ((section(".endof"))) _flash_size ;
but the compiler says undefined reference.
2020-04-08 2:33 PM
>>just curious, why "_limit_flash - g_pfnVector" is done both in startup and linker files?
Because I wanted to use _flash_size, but the stupid GNU linker doesn't do the relocation/math properly when it binds startup.s, and I wasn't willing to debug the linker.
>>i am trying extern uint32_t __attribute__ ((section(".endof"))) _flash_size ;
It is not a variable with an address, it is a linker symbol, that's why I put the size in a memory location within the vector table.
2020-04-08 5:03 PM
well how do i access the vector table from the code? i looked at .map file. it shows this
.isr_vector 0x0000000008000000 0x184
0x0000000008000000 . = ALIGN (0x4)
*(.isr_vector)
.isr_vector 0x0000000008000000 0x184 Startup/startup_stm32f207vetx.o
0x0000000008000000 g_pfnVectors
0x0000000008000184 . = ALIGN (0x4)
.crc32 0x0000000008010000 0x4
*(.crc32)
.crc32 0x0000000008010000 0x4 Src/main.o
0x0000000008010000 crc_crc32so i think that my firmware length will be at the top of memory, but
none of these values are of firmware size. text + data from :
arm-none-eabi-size SGW.elf
arm-none-eabi-objdump -h -S SGW.elf > "SGW.list"
arm-none-eabi-objcopy -O binary SGW.elf "SGW.bin"
text data bss dec hex filename
191800 564 110424 302788 49ec4 SGW.elfwhat i am doing wrong here?
2020-04-08 5:36 PM
extern uint32_t *g_pfnVectors[];
printf("%p %p\n",g_pfnVectors[0], g_pfnVectors[1]);
2020-04-09 3:33 AM
Thank you so much. it works.