cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to use the STM32 Cryptographic library on a ECOM10?

GCorr.2
Associate II

Hi, I'm new in the forum and I would like to have your technical support. 

Unfortunately regarding this topic I was not able to found info in internet, and I don't know if I'm trying to do something not allowed by the ST libraries.

For my application I need the SHA256 and RS2048 algorithms.

The mcu is an ECOM10, while the IDE is IAR v.8.3.

Considering that ECOM10 integrate a Cortex M4F, I tried to use the libraries for the STM32F4 family. Is that choice right? 

In particular I tried to use without success both:

1) STM32_Cryptographic_Library_V2.0.6

2) STM32CubeExpansion_Crypto_V3.1.0

For the "STM32_Cryptographic_Library_V2.0.6", I was able to build the project only using the "M4_CryptoHW_2_0_6.a", i.e. with the hw accelleration.

While for the "STM32CubeExpansion_Crypto_V3.1.0", I was able to build the project using both "STM32CryptographicV3.1.1_CM4_IARv8" and "STM32CryptographicV3.1.1_CM4_IARv8_otnsc.a".

For all cases, I've used as reference the sha256 project example, but unfortunately all the test failed, I always got a wrong digest value.

Aspected digest: 248D6A61D20638B8E5C026930C3E6039A33CE45964FF2167F6ECEDD419DB06C1

Calculed digest: DE455CD3C0D51251E2A2066AF6ACE2554FA67B4E3500EDE374AEA19D4FE0B5EC

Any suggestions is more than welcome.

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

The libraries are locked to STM32 parts, they fail if the detect other hardware.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi thanks for the fast reply. It seems that is not failing, because the error status returned is HASH_SUCCESS. Only the calculated value is wrong. Or do you think that this could happen also in case of other hardware detection?

I'd class returning the wrong hash a mode of failure.

​

You'll need to use your own library, or discuss the issue with the ST support engineers responsible for your account.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Ok thanks a lot.