2020-12-15 10:56 PM
I have a routine that I have used for years on other processors and on PCs to get a CRC16 X-25 from a string. I'd like to get the hardware CRC to use the same CRC16.
I have tried every variant in the STM32CubeIDE and have not been able to get same output.
I know the X-25 uses an XOR of 0xFFFF which I do to the result I get from the HAL_CRC_Calculate.
I'm using my name as the test string...
unsigned char crcTest[]="Jim Fouch";
and then calling the CRC in HAL like this...
crcResult = ~HAL_CRC_Calculate(&hcrc, (uint32_t *)&crcTest, strlen(crcTest));
Here is my crc Init...
static void MX_CRC_Init(void)
{
/* USER CODE BEGIN CRC_Init 0 */
/* USER CODE END CRC_Init 0 */
/* USER CODE BEGIN CRC_Init 1 */
/* USER CODE END CRC_Init 1 */
hcrc.Instance = CRC;
hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_DISABLE;
hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_DISABLE;
hcrc.Init.GeneratingPolynomial = 4129;
hcrc.Init.CRCLength = CRC_POLYLENGTH_16B;
hcrc.Init.InitValue = 0xFFFF;
hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
if (HAL_CRC_Init(&hcrc) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CRC_Init 2 */
/* USER CODE END CRC_Init 2 */
}
Which according to my coded routine and an online CRC test util, should return 0x0BAD. I know it's funny that my name returns "BAD" as a hex result. LOL
Here is the util I'm using... www.crccalc.com
Looking for any help. I'm sure I'm overlooking something.
2020-12-15 11:33 PM
Which STM32?
Drop Cube and feed the CRC byte-wise, as the first experiment, then try halfwords with various control bits settings.
JW
2020-12-16 12:02 AM
STM32H743
2020-12-16 12:20 AM
Figured it out.
Needed to Invert In & Out...
hcrc.Instance = CRC;
hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_DISABLE;
hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_DISABLE;
hcrc.Init.GeneratingPolynomial = 4129;
hcrc.Init.CRCLength = CRC_POLYLENGTH_16B;
hcrc.Init.InitValue = 0xFFFF;
hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_BYTE;
hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_ENABLE;
hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
and then invert the CRC
crcResult = ~HAL_CRC_Calculate(&hcrc, (uint32_t *)&crcTest, strlen(crcTest));
2021-04-14 2:16 PM
Thank you for posting, have been struggling trying to get the HW crc calculator to produce the correct result and this got is working
This is what i needed for 16 bit CRC:
hcrc.Instance = CRC;
hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_DISABLE;
hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_DISABLE;
hcrc.Init.GeneratingPolynomial = 0x1021;
hcrc.Init.CRCLength = CRC_POLYLENGTH_16B;
hcrc.Init.InitValue = 0xFFFF;
hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_HALFWORD;
hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_ENABLE;
hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_HALFWORDS;
if (HAL_CRC_Init(&hcrc) != HAL_OK)
{
Error_Handler();
}
and in my case, no inversion needed on out put:
uint8_t data[] = {0, 1, 2, 3, 4, 5, 6, 7};
uint32_t hal_crc = HAL_CRC_Calculate(&hcrc, (uint32_t *)data, 4);
gets correct crc of 0x9DFD