BOOT_LOCK not cleared?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-03-06 11:09 AM
Hello,
RM0444.Rev5 page 98 says that it is possible to reset it only when:
• RDP is set to Level 0, or
• RDP is set to Level 1, while Level 0 is requested and a full mass-erase is performed.
I supposed that if RDP is changed from level1 to level0 then the BOOT_LOCK is also automatically removed after the mass-erase triggered by that RDP change.
Is that correct?
This is not what I see with STM32CubeProgrammer v2.10.0 and stm32g031 chip because I have to manually remove it in a successive step.
Thank you.
Solved! Go to Solution.
- Labels:
-
STM32 Security
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-03-06 11:27 AM
Hello @S-.1
After regression from Level 1 to Level 0, the BOOT_LOCK bit is not automatically removed. But, you need to reset it manually according to the description on the RM0444.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-03-06 11:27 AM
Hello @S-.1
After regression from Level 1 to Level 0, the BOOT_LOCK bit is not automatically removed. But, you need to reset it manually according to the description on the RM0444.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.