2023-08-24 4:53 AM
Hello,
I'm using AES-GCM using the method cmox_cipher_append() function call, as taken from the example below, taken from Projects\NUCLEO-L476RG\Applications\Cipher\AES_GCM_AEAD_EncryptDecrypt\Src\main.c
The code works well if the CHUNK_SIZE size is a multiple of 16. However, I want to decipher streamed data that comes in unpredictable chunks. I know that there is no limitation from the AES-GCM algorithm side on the CHUNK_SIZE. Is there a workaround to implement something with a CHUNK_SIZE of 1?
2023-09-08 3:28 PM - edited 2023-09-12 10:39 AM
Hello Michael,
Your inquiry has been escalated to the ST Online Support team for direct support.
In the future, for prioritized support please submit directly to https://my.st.com/ols.
Kind Regards,
Christian
ST Support
2023-09-13 9:52 AM
Hello Michael,
I confirm here that the X-CUBE-CRYPTOLIB 4.1.0 does not support CHUNK_SIZE of 1 if this is not the end of the cyphertext, and there is no workaround to get this BYTE level decryption. (Same for encryption)
I created a change request which is currently under analysis.
Best regards
Jocelyn
2024-05-02 10:59 AM
Any update on this
2024-05-03 11:53 AM
Hello @Rajan Soma ,
the change request has been included in the development plan.
Now I couldn't get any committed date for this change.
One point to know it that such change will require a new certification of the library which is not something we want to do too often ...
Best regards
Jocelyn