2024-07-23 06:43 AM
Hello,
I want to use the GFX02Z1 shield with my Nucleo H743ZI2.
To discover the product I'm trying to run the Hello_World example application from X-CUBE-DISPLAY Software Pack Component that I downloaded.
Here is how I configured X-CUBE-DISPLAY:
I tried to use these documentations:
and
Now, I have two issues:
- I dont know how to configure the Parameter Settings menu (no information in the documentation)
- I don't know how to configure the Platform Settings menu because the documentation doesn't precise the PIN I should use for SPI
(I just managed to make the joystick works) from this table
But I don't understand what SPI / GPIO I should use for the MX25L6433F memory and the ILI9341 screen.
Any help would be well appreciated,
Thanks
2024-07-24 12:40 AM - edited 2024-07-29 04:15 AM