2017-12-26 03:49 AM
Hi, I have these two shields and I want to integrate their libraries into a code generated by CubeMX where USBhost and FATFS middleware with relative pins are defined. I think that Shields' libraries are available only on their evaluation programs, such as SOUNDTER1_V2.0.0 for CCA01M1, aren't them? So, Are there some rules to follow in order to link these libraries? I use EWARM to develop. The board is F401RE.
Thanks a lot, best regards
#cubemx-project #nucleo-f401 #x-cube-soundter1 #x-cube-cca01m1