cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong timer section identifier in manual (G431RBT6)

Tobe
Senior III

I think there are some wron identifiers?

After reading the manual and seeing the tables i think it must be "tim_ti2_in0", "tim_ti3_in0" and "tim_ti4_in0" on page 1223?

 

Also in the table on page 1081, there is a "tim_ti2_in[15:1]" that should be "tim_ti3_in[15:1]".

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello @Tobe,

The first reported typo is fixed in the latest RM0440 Rev 8.

ImenD_0-1712606029731.png

- About the second typo: You are right. 

There is a "tim_ti2_in[15:1]" on Table 250. Interconnect to the tim_ti3 input multiplexer, and this should be "tim_ti3_in[15:1]".

ImenD_0-1712606219393.png

I escalated this internally for fix within internal ticket number 178513 (This is an internal tracking number and is not accessible or usable by customers)

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen