cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong reference temperature given in ds H747

AScha.3
Chief III

Hi,

in ds for STM32H747xI/G  , DS12930 Rev 2 , for Temp.sensor CAL2 : 130° (Parameter) is written here:

 

AScha3_0-1721813254582.png

BUT  max. temp for chip is 125° :

AScha3_1-1721813336011.png

So i assume, this is misspelled  , because in all other : (H743, H750, H7A3 ..) 110° + 30° are given.

NOT 130° .

 

 

 

If you feel a post has answered your question, please click "Accept as Solution".
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee


Hello @AScha.3 

I can confirm that the TS_CAL2 value has been taken for 130° on the STM32H747xI/G. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee


Hello @AScha.3 

I can confirm that the TS_CAL2 value has been taken for 130° on the STM32H747xI/G. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.