2020-09-03 7:25 AM
I need to write to the 4kB battery backed SRAM to hold information across power cycles, but it's not working! To be more specific:
Here's my code for writing to BB SRAM:
// Now write it to BB SRAM
RCC->APB1ENR |= RCC_APB1ENR_PWREN; // Enable power interface clock by setting the PWREN bit
PWR->CR1 |= PWR_CR1_DBP; // Disable write protection
RCC->AHB1ENR |= RCC_AHB1ENR_BKPSRAMEN; // Enable the backup SRAM clock by setting BKPSRAMEN
__DMB();
memcpy((void *)pSRAM, &pay, len + sizeof(uint16_t));
__DMB();
SCB_CleanDCache();
reg = RCC->AHB1ENR; // definig reg as volatile forces a read
RCC->AHB1ENR &= ~RCC_AHB1ENR_BKPSRAMEN;
PWR->CR1 &= ~PWR_CR1_DBP;
RCC->APB1ENR &= ~RCC_APB1ENR_PWREN;As you can see, I'm throwing everything at beating the cache but still no joy.
Solved! Go to Solution.
2020-09-03 4:10 PM
When the backup domain is supplied by V BAT (analog switch connected to V BAT because
V DD is not present), the backup SRAM is powered by a dedicated low-power regulator. This
regulator can be ON or OFF depending whether the application needs the backup SRAM
function in Standby and V BAT modes or not. The power-down of this regulator is controlled
by a dedicated bit, the BRE control bit of the PWR_CSR1 register
Quoting from 'F746 RM as I was lazy to download a 'F767 RM, but it will be the same.
JW
2020-09-03 4:10 PM
When the backup domain is supplied by V BAT (analog switch connected to V BAT because
V DD is not present), the backup SRAM is powered by a dedicated low-power regulator. This
regulator can be ON or OFF depending whether the application needs the backup SRAM
function in Standby and V BAT modes or not. The power-down of this regulator is controlled
by a dedicated bit, the BRE control bit of the PWR_CSR1 register
Quoting from 'F746 RM as I was lazy to download a 'F767 RM, but it will be the same.
JW
2020-09-04 12:42 AM
Power-cycle is NOT the same as reset.
Reset just sets specific things to certain states. Anything else is left unchanged.
Power-cycle means any other RAM values could be in random states. If you only lost power for a short time, many of the bits in RAM could be unchanged. But losing power for a longer time means that a higher proportion of bits will be scrambled.
How strongly do you know that it is the cache you are having to fight? Does it (for example) work if you never enable the data cache?
You have not shared the code of where you try to read the backup SRAM. Do you make sure you have enabled RCC->AHB1ENR |= RCC_AHB1ENR_BKPSRAMEN; beforehand?
Hope this helps,
Danish
2020-09-04 1:45 AM
Jan, that looks like it! It's taken me a while to figure out what's stopping me from turning BRE on! I can't see it in the manual but you need to set PWR->CR1 DBP before you can set BRE.
BTW did you use to hang out on www.8052.com?
2020-09-04 1:48 AM
Hi Danish, thanks for your input. I'm well aware of the differences between Reset and a power cycle, but that's kind of the point of battery backed RAM. I didn't post read code because reads work fine and my code and the debugger agree on what's in there.
2020-09-04 2:29 AM
2020-09-04 2:32 AM
> Now I just need to figure out what's stopping me from turning BRE on!
Do you have enabled clock for PWR in RCC?
You may perhaps also want to add some delay after the clock enable, before accessing PWR.
JW
2020-09-04 2:41 AM
From what I can see, you say that when you write then read back, what you wrote was read back correctly.
But when you read back before having written (for the value to persist over reset and power-down-with-battery-backup) you do not read the last-stored value.
So what I was raising was the possibility that the write, or other things that happen leading up to the write, leave the processor and its peripherals in a state where it is able to read things back.
What value do you read when it doesn't work? Is it always the same value?
The data cache won't give a cached value if (since the reset) that memory-location has never been read.
You might get a value suggests "there's no peripheral at this memory location" if you've never enabled power/access to the BBSRAM or never enabled its clock.
But you might also get a value e.g. 0 that suggests that your C compiler is unhelpfully clearing out memory for all static variables prior to entering main().
2020-09-04 3:00 AM
I've edited my earlier post, but just to re-iterate you need to set DBP in CR1 before you can set BRE
2020-09-04 3:03 AM
Hi Danish, Jan's put his finger on it. I have to say the protection ST put on the BB SRAM is seriously strong and I re-enable it after I've done the write.
Thanks for your thoughts, appreciated.