2025-01-24 05:33 AM - last edited on 2025-01-24 05:48 AM by Andrew Neil
Hi everyone
I'm using a STM32F401RCT6 to control a valve actuator
There is a counter of number of cycles for the actuator (RunTime), and when its value changes, the value of that counter must be stored in the memory for tracking and support.
The actuator is powered by an external power supply and additionally there's a battery in case the power fails.
In some rare cases, the memory storage process is corrupted, and we lose the complete storage values previously saved.
We are trying to replicate the fail, but it is really impossible
Do you have any idea of what can cause that loss of information in the memory and how could we replicate this failure in order to fix the bug
below is part of the code that writes to memory
Thank you very much
int WriteToFlash(bool force)
{
uint8_t NibleH=0;
uint8_t NibleL=0;
int16_t AuxData=0;
uint32_t Variable_Guardar;
uint32_t PAGError = 0;
FLASH_EraseInitTypeDef EraseInitStruct;
if((Entrada_Control_Seleccionada!=Problem || force) && Scale.VoltMain >20 ) //Force write in memory when a fail occurs
{
/* Fill EraseInit structure*/
EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
EraseInitStruct.Banks = FLASH_BANK_1;
EraseInitStruct.Sector = FLASH_SECTOR_1;
EraseInitStruct.NbSectors = 1;
EraseInitStruct.VoltageRange = FLASH_VOLTAGE_RANGE_3;
HAL_FLASH_Unlock();
// Erase the USER_FLASH
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGError) != HAL_OK)
{
return 1;
}
// Write the delay value in flash memory //0x5051
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1, 0x5051) != HAL_OK)
{
return 1;
}
Index.Modo_Entrada=Entrada_Control_Seleccionada_M;
Variable_Guardar=AjustarDatos_8bits_ParaBackUp(0,0,Index.Modo_Entrada,Index.ModeWork);
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+4, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;
}
AuxData=Scale.Temp_SP;//Save Anticondensation temperature value
NibleL=0xFF & AuxData;
NibleH=AuxData>>8;
Variable_Guardar=AjustarDatos_8bits_ParaBackUp(0,0,NibleH,NibleL);
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+8, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;
}
Variable_Guardar=AjustarDatos_8bits_ParaBackUp(Index.FactorScal,TEMP_AlmHH,Index.LED,Index.Modo_Giro); //Save setting TEMP_AlmHH
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+12, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;
}
Variable_Guardar=AjustarDatos_8bits_ParaBackUp(0,0,Index.LED_Update,Index.SP_Fault_Power); //LFH, 2023/05/26 Ver 2.1.0: Save setting LED_Update (indicate the state for the LED)
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+16, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;
Variable_Guardar=RunTime;
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, (uint32_t) &BackUp_1+88, Variable_Guardar) != HAL_OK)
{
HAL_FLASH_Lock();
return 1;
}
.
.
.
HAL_FLASH_Lock();
return 0;
}else{
return 1;
}
}
Solved! Go to Solution.
2025-01-25 02:54 AM
For Emulating EEPROM in Flash on STM32F4, ST provide the STSW-STM32066 software pack, EEPROM emulation in STM32F40x/STM32F41x microcontrollers:
https://www.st.com/en/embedded-software/stsw-stm32066.html
See Application Note AN3969, EEPROM emulation in STM32F40x/STM32F41x microcontrollers for details:
https://www.st.com/en/embedded-software/stsw-stm32066.html#documentation
@Alejandra It may not exactly suit your requirements, but it does show how to use the STM32F4 Flash for data storage.
With that knowledge, you could adapt to your own needs; eg, see:
https://community.st.com/t5/stm32-mcus-embedded-software/eeprom-emulation-virtual-addresses/m-p/675964/highlight/true#M47888
and follow the link.
2025-01-24 01:07 PM
Resetting the chip or removing power during a flash write operation can cause corrupted/incomplete data stored. That's most likely. Also possible is insufficient power for the chip, such as using operations that require 3.3V when you are only supply 2.7V.
2025-01-25 02:36 AM
Aside all suggestions in @TDK post that I do totally agree, I would rise some more concerns.
Flash is NOT designed to be used as you are planning; tipically EEPROMS are the solution for incremental data storage.
But if you are unable to force hw design change, you must handle Flash as unreliable storage media.
This means using data buffering and performing readback checks for correct storage content before deleting data:
Another concerns is relate to Flash lifecycle.
Check on datasheet if minimum number of cycles is enough for your application; do not allow products to go out and have some percentage of them undeperform.
2025-01-25 02:54 AM
For Emulating EEPROM in Flash on STM32F4, ST provide the STSW-STM32066 software pack, EEPROM emulation in STM32F40x/STM32F41x microcontrollers:
https://www.st.com/en/embedded-software/stsw-stm32066.html
See Application Note AN3969, EEPROM emulation in STM32F40x/STM32F41x microcontrollers for details:
https://www.st.com/en/embedded-software/stsw-stm32066.html#documentation
@Alejandra It may not exactly suit your requirements, but it does show how to use the STM32F4 Flash for data storage.
With that knowledge, you could adapt to your own needs; eg, see:
https://community.st.com/t5/stm32-mcus-embedded-software/eeprom-emulation-virtual-addresses/m-p/675964/highlight/true#M47888
and follow the link.
2025-02-03 05:30 AM
Thank you Andrew
The Application Note AN3969, gave an idea of how to avoid that error with EEPROM emulation
Although we also found a issue due to ground connectivity between the PLC and the actuator
I really appreciate your suggestion