cancel
Showing results for 
Search instead for 
Did you mean: 

Would like to use the UART on the STM32F429ZIT Discovery boart

kartik
Associate II
Posted on April 04, 2014 at 03:22

I would like to use one of the UARTS on the STM32F4 to connect the MCU to a Bluetooth SMART controller. I was wondering if anyone could tell me if there is any access on the board to one of the UARTs so that i can solder wires to pull the RX/TX lines out. If so, which UART is it? I'm sure going through the schematic would tell me this, but I'm a noob to the really lowlevel embedded stuff and I've been looking at the schematic for a while and still can't figure it out. Any help would be much appreciated.

Thanks

Kartik

#discovery #uart #stm32f4
2 REPLIES 2
Posted on April 04, 2014 at 20:07

Have you looked at the schematics?

Posted on April 04, 2014 at 20:48

The manual for the STM32F429I-DISCO does enumerate a pin list, if you can't decode the schematic this list would be where to start.

As I recall USART1 PA9/PA10 are available on this board.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..