2021-10-08 04:43 AM
Hi guys
I have a real strange issue
trying to move two 8bits values in to one 16bit variable,
can someone please tell me why this does not work
It should OR the lsb to the msb
Sensor_Flow = I2C1_DATA[0] ;
Sensor_Flow = Sensor_Flow << 8;
Sensor_Flow = Sensor_Flow || I2C1_DATA[1];
thanks in addvance
Solved! Go to Solution.
2021-10-08 07:25 AM
Simpler, less prone to be wrong..
Sensor_Flow = ((uint16_t)I2C1_DATA[0] << 8) + (uint16_t)I2C1_DATA[1];
2021-10-08 04:55 AM
Hi,
you mixed up || (logical OR) and | (binary OR), please try :
Sensor_Flow = Sensor_Flow | I2C1_DATA[1];
assuming I2C1_DATA[ ] is defined as bytes array, otherwise need to mask to get only LSByte (i.e. I2C1_DATA[x] & 0xFF) .
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2021-10-08 04:56 AM
if sensor_flow is uint16_t and I2C_DATA is a uint8_t or char array....
you could also try
memcpy(&Sensor_Flow, &I2C_DATA[0],2);//2=2bytes
2021-10-08 05:51 AM
Thanks guys
Just coming back to C after a long break,
Doh back to the drawing board :-(
Regards
2021-10-08 06:10 AM
Hi guys
don't think mem copy will work as my first byte of data [0] is the msb and byte 2 [1] is lsb
It create the 16bit data variable with the byte order wrong
though I like the simplistic approach
Regards
2021-10-08 07:25 AM
Simpler, less prone to be wrong..
Sensor_Flow = ((uint16_t)I2C1_DATA[0] << 8) + (uint16_t)I2C1_DATA[1];