Why is there so much latency in my interrupt?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-15 2:28 AM
I am working with the STM32 Nucleo-64 development board, which has an STM32L476R microcontroller. My SystemCoreClock is 16 MHz and TIM17 is clocked at 4 MHz. To my surprise, the code below only works well (the timer doesn't miss the next interrupt and wraps around) if I increment with at least 23:
#pragma GCC push_options
#pragma GCC optimize ("O3")
void TIM1_TRG_COM_TIM17_IRQHandler(void) {
GPIOC->BSRR = 0x00000400; // Set test pin PC10 high
GPIOC->BSRR = 0x04000000; // Set test pin PC10 low
TIM17->SR = 0; // Clear interrupt flags
TIM17->CCR1 += 23; // OK
// TIM17->CCR1 += 22; // Not ok
}
#pragma GCC pop_options
Now, 23 timer ticks corresponds to 23 x 4 = 92 CPU clock cycles and it seems unlikely that the 4 lines of code would occupy 92 instructions. When I store the TIM17->CNT value in a global variable first thing in the interrupt routine above I can see that TIM17->CNT is 8 (!) more than TIM17->CCR1 meaning it took roughly 8 x 4 = 32 CPU clock instructions just to enter the interrupt routine! I tried to put the interrupt vector in RAM, but that made it worse! What am I doing wrong, why is there so much latency in my interrupt?
Solved! Go to Solution.
- Labels:
-
Interrupt
-
STM32L4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 4:55 AM
Please see my correction above and apologize for misleading you.
> if I modify my code and store TIM17->CNT into a global variable (not a stack variable)
> first thing in the interrupt routine, then it is 8 more than TIM17->CCR1,
> meaning it takes 8 x 4 = 32 CPH clock cycles until the first line of code is executed.
Always post disasm; "first line" of C is irrelevant in context of cycle counting.
Also, read out and post RCC and FLASH-relevant registers content, to have some firm base for further discussion. For what I take from
>>> SystemCoreClock is 16 MHz and TIM17 is clocked at 4 MHz.
>>Are you sure?
> Yes
it means that APB on which the timer sits is clocked at 2MHz, i.e. 8 AHB cycles per one APB cycle, correct?
Then read section from my post above above, containing "... accessing registers in timer (i.e. through the /4 APB bus) impose delays ..." and the post I've linked there.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 8:19 AM
These are the clock settings I'm using:
This is my code when I sample TIM17->CLK asap in the interrupt routine:
static int timerCntValue;
void TIM1_TRG_COM_TIM17_IRQHandler(void) {
timerCntValue = TIM17->CNT;
802eec0: 4b0d ldr r3, [pc, #52] ; (802eef8 <TIM1_TRG_COM_TIM17_IRQHandler+0x38>)
802eec2: 490e ldr r1, [pc, #56] ; (802eefc <TIM1_TRG_COM_TIM17_IRQHandler+0x3c>)
802eec4: 6a58 ldr r0, [r3, #36] ; 0x24
TOGGLE_TEST_PIN_1();
802eec6: 4a0e ldr r2, [pc, #56] ; (802ef00 <TIM1_TRG_COM_TIM17_IRQHandler+0x40>)
void TIM1_TRG_COM_TIM17_IRQHandler(void) {
802eec8: b410 push {r4}
timerCntValue = TIM17->CNT;
802eeca: 6008 str r0, [r1, #0]
TOGGLE_TEST_PIN_1();
802eecc: f44f 6480 mov.w r4, #1024 ; 0x400
802eed0: f04f 6080 mov.w r0, #67108864 ; 0x4000000
TIM17->SR = 0; // Clear interrupt flags
If I don't make a function call inside the interrupt routine, timerCntValue will be assigned the threshold TIM17->CCR1 plus 5 timer ticks. If I call a function (e.g. send the timerCntValue value to a UART) then timerCntValue will be TIM17->CCR1 plus 8 timer ticks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 8:45 AM
> I don't make a function call inside the interrupt routine, timerCntValue will be assigned the threshold
> TIM17->CCR1 plus 5 timer ticks.
So 20 system clocks. That's consistent with 12 system clocks of ISR latency + 2 system clocks to load r3 and r1 from FLASH + (0..7) + 8 system (AHB) clocks to get through the AHB/APB bridge with APB running at AHB/8 in order to load r0 from TIM_CNT. Give or take a couple of clocks, for I don't know exactly how things are synchronized.
JW

- « Previous
- Next »