2017-11-09 5:16 AM
I want to protect a memory region from writing. I've configured MPU, but it is not generating any faults.Please help.
Here are the registers configuration:
MPU_RNR = 0x00000000; // using region 0
MPU_RBAR = 0x20000000; // base address is 0x20000000 MPU_RASR = 0x0700110B; // Size is 64 bytes, no sub-regions, permission = 7(ro,ro), s=b=c=tex=0 MPU_CTRL = 0x00000001; // enable MPUNow when I write in this region of memory, it does not generate any exception and writes successfully.
__asm(
'LDR R0, =0x20000000\n\t' // load address in r0, 0x20000000 'MOV R1, 0x77777777\n\t' 'STR R1, [R0,&sharp0]' // write to address 0x200000000 );This is the definition of handler:
void MemManage_Handler(void)
{ __asm( 'MOV R4, 0x77777777\n\t' 'MOV R5, 0x77777777\n\t' );}I am writing to r4 and r5 just to make sure if the handler was executed or not. This has nothing to do with the rest of the program.
Here's a complete source code:
&sharpdefine MPU_CTRL (*((volatile unsigned long*) 0xE000ED94))
&sharpdefine MPU_RNR (*((volatile unsigned long*) 0xE000ED98))&sharpdefine MPU_RBAR (*((volatile unsigned long*) 0xE000ED9C))&sharpdefine MPU_RASR (*((volatile unsigned long*) 0xE000EDA0)) void Registers_Init(void){MPU_RNR = 0x00000000;
MPU_RBAR = 0x20000000; MPU_RASR = 0x0700110B; MPU_CTRL = 0x00000001;}void MemManage_Handler(void)
{ __asm( 'MOV R4, 0x77777777\n\t' 'MOV R5, 0x77777777\n\t' );}int main(void)
{ Registers_Init(); __asm( 'LDR R0, =0x20000000\n\t' 'MOV R1, 0x77777777\n\t' 'STRD R1, [R0,&sharp0]' ); return (1);}void SystemInit(void)
{}#programming #mpu #keil-uvision #fault-exception #stm32f103rb #memmanage-hard-fault2017-11-09 6:48 AM
Is the exception enabled with
SCB->SHCSR = 0x01 << 16;
NVIC_EnableIRQ (MemoryManagement_IRQn);
?
Can you share the full source code ?
2017-11-09 8:17 AM
>>
Can you share the full source code ?
Or at least the smallest free standing and compiling code that demonstrates/illustrates the issue, and the test case.
2017-11-09 9:21 AM
Thanks for reply. I've shared the source code.
2017-11-09 9:25 AM
I've shared the source code. Thank u.
2017-11-09 10:18 AM
So, seems that the MemManage fault is not enabled and will therefore default to HardFault. See
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0552a/Cihieffb.html
.Also,
MemoryManagement_IRQn
seems not to be enabled in the NVIC.2017-11-09 10:50 AM
How do I enable MemoryManagement_IRQ in NVIC? I've enabled the
MemManage fault from
System Handler Control and State Register, and it's still not working. So kindly tell me how do I use NVIC?
2017-11-09 11:04 AM
I've reported this above: you can use CMSIS call
NVIC_EnableIRQ (MemoryManagement_IRQn);
2017-11-09 1:17 PM
Thanks. Lastly, is there any problem with my registers configuration?
2017-11-10 12:42 PM
Nope, everything looks fine.
Double check with the enclosed file which triggers MPU fault on a STM32L
________________ Attachments : mpu-test.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hy9y&d=%2Fa%2F0X0000000b5s%2F4P0xnoEeeFavMwdZkfaWSNrx0r5Kt69u4LuDuNPv8K0&asPdf=false