cancel
Showing results for 
Search instead for 
Did you mean: 

Why does STM32F4 DAC have left or right data alignment in 12-bit mode? What is that supposed to mean?

Andrew C
Associate III

In the datasheet, it says that the DAC has left or right data alignment in 12-bit mode. What is this mode supposed to do? Also, it says "8-bit or 10-bit monotonic output". Does that mean in 12 bits, it is no longer monotonic?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
T J
Lead

The top 8 bits are useful,

sometimes, its all you need,

hence the right justification...

to dump the bottom bits of noise....

It means it fills upper or lower bits depending on the user's application and needs.

If you want to do signed math you kind of want the data in the high order bits, or for example the interface they get sent over has different bit widths and discards low order bits. ie 12-bit data into a 10-bit codec.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..