Why do I get an Error after stetting the PLL as System clock input?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-04 3:04 PM
This is the code:
#include <stm32f4xx.h>
void main(void)
{
//Set up PA5(LED)
RCC -> AHB1ENR |= 0x00000001; //enables clock for GPO PA
GPIOA -> MODER |= 0x00000400; //PA Pin 5 as GPO
GPIOA -> OTYPER |= 0x00000000; //PA Pin 5 as Push/Pull
GPIOA -> OSPEEDR |= 0x00000C00; //PA Pin 5 as High speed
GPIOA -> PUPDR |= 0x00000000; //PA Pin 5 as No pull-up/down
//clock at 180mhz
RCC -> PLLCFGR &= ~(1<<22); //set HSI as PLL input
RCC -> PLLCFGR |= (1<<4); //set PLLM prescaler to 16
RCC -> PLLCFGR |= ((1<<9) | (1<<11) | (1<<12) | (1<<14)); //PLL multimpiler *360
RCC -> CFGR |= ((1<<10) | (1<<12)); //AHB1 presclaer = /4
RCC -> CFGR |= (1<<12); //AHB2 prescaler = /2
RCC -> CR |= (1<<24); //enables PLL
RCC -> CFGR |= (1<<1); //sets PLL as main clock input
while(1)
{
//main loop
GPIOA -> BSRR = (1<<5);
GPIOA -> BSRR = (1<<21);
}
}
Once I start the code and it gets to RCC -> CFGR |= (1<<1); I get an error. I do not see why? Can someone please explain me? I am using the Segger IDE. All code is written in C. It should configure the Main PLL to get the freq. from the HSI and get it to 180MHz. Once the code gets to the point where it changes the system clock source from HSI to PLL _P it crashed:
Loading target script file STM32F4xx_Target.js
Preparing target for download
Executing Reset script Reset();
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Downloading ‘blink.elf’ to J-Link
Programming 1.1 KB of addresses 08000000 — 080004c7
J-Link: Flash download: Bank 0 @ 0x08000000: 1 range affected (16384 bytes)
J-Link: Flash download: Total time needed: 0.525s (Prepare: 0.066s, Compare: 0.041s, Erase: 0.374s, Program: 0.026s, Verify: 0.008s, Restore: 0.008s)
Download successful
T-bit of XPSR is 0 but should be 1. Changed to 1.
Stopped by vector catch
Error reading from memory
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-04 3:20 PM
You need to increase number of waitstates for reading from FLASH, LATENCY in FLASH_ACR.
For 180MHz, you need also to switch on "overdrive", see ODEN bit of PWR_CR register.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-04 3:20 PM
You need to increase number of waitstates for reading from FLASH, LATENCY in FLASH_ACR.
For 180MHz, you need also to switch on "overdrive", see ODEN bit of PWR_CR register.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-04 4:11 PM
Hey,
thank you for your quick response.
It fixed the error, but
it only works when I dont check the status registers.
From datasheet:
Entering Over-drive mode:
3. Set ODEN bit of PWR_CR register to enable the Over-drive mode and wait for the
ODRDY flag to be set in the PWR_CSR register.
My Code:
PWR -> CR |= (1<<17); //enables overdrive mode
while(!(PWR->CSR&(1<<17))); //checks for overdrive mode enabled
If i leave out the while loop everything works, but as soon as I put it back in the code gets stuck in that loop
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-04 4:12 PM
Hey,
thank you for your quick response.
It fixed the error, but
it only works when I dont check the status registers.
From datasheet:
Entering Over-drive mode:
3. Set ODEN bit of PWR_CR register to enable the Over-drive mode and wait for the
ODRDY flag to be set in the PWR_CSR register.
My Code:
PWR -> CR |= (1<<17); //enables overdrive mode
while(!(PWR->CSR&(1<<17))); //checks for overdrive mode enabled
If i leave out the while loop everything works, but as soon as I put it back in the code gets stuck in that loop
Complete new Code:
RCC -> PLLCFGR &= ~(1<<22); //set HSI as PLL input
RCC -> PLLCFGR |= (1<<4); //set PLLM prescaler to 16
RCC -> PLLCFGR |= ((1<<9) | (1<<11) | (1<<12) | (1<<14)); //PLL multimpiler *360
RCC -> CR |= (1<<24); //enables PLL
PWR -> CR |= (1<<17); //enables overdrive mode
while(!(PWR->CSR&(1<<17))); //checks for overdrive mode ready
FLASH -> ACR |= ((1<<0) | (1<<2)); //5 wait states
RCC -> CFGR |= ((1<<10) | (1<<12)); //AHB1 presclaer = /4
RCC -> CFGR |= (1<<12); //AHB2 prescaler = /2
while(!(RCC->CR&(1<<25))); //checks for pll lock
RCC -> CFGR |= (1<<1); //sets PLL as main clock input
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-04 8:40 PM
Bit 17 is overdrive mode switching bit. Bit 16 is overdrive mode enable. That's if your chip is F42x or 43x. F40x and F41x don't have those bits.