2025-10-13 11:53 PM - last edited on 2025-10-14 2:03 AM by Andrew Neil
In the Datasheet, Table 16 specifies TJMAX as 150 °C, but Table 17 indicates the TJ range as -40~130 °C, which one should I refer to?
Table 16. Thermal characteristics
Symbol Ratings Value Unit
TSTG Storage temperature range –65 to +150 °C
TJ  Maximum junction temperature 150 °C
Table 17. General operating conditions
TJ Junction temperature range Suffix 6 version -40 105 °C Suffix 3 version -40 130
Solved! Go to Solution.
2025-10-14 2:32 AM
Understood, thank you for the response.