2017-06-20 1:09 AM
I would like to build a project based on STM32 that interfaces with a CAN network. The CAN network has a 250kbps baud rate.
On this network I have to:
I was thinking of using an STM32 with 2 CANs. My intention is to set up 2 different filters on IDs and limit interruptions. Is that a good choice? Can it be done with only one CAN?
I have doubts about the kind and the speed of processor to use. Can an STM32F1/F0 be sufficient? Or do I need an F4?
Thanks in advance.
2017-06-20 3:39 AM
Whether or not to use 2 CAN interfaces depends on how you are connecting to the network. If there's only one bus adding a second transceiver and interface won't help performance. You are limited by the bandwidth of the bus itself, not the controller. If it's a dual bus, something like an ISOBUS tractor or combine, then you must have 2 separate bus transceivers and interfaces.
Unless youa re building a large number of these repeaters I'd recommend an F4, only because it gives you some margin in terms of memory buffers. Bear in mind you may have to keep a large buffer of messages in case of heavy contention or a node failure, which can temporarily take the bus offline.
Otherwise your application is basically a store and forward repeater, not a complex task. Performance is limited by how much access time you can get on the bus, not the controller core. If it's cost sensitive look at an F2.
Jack Peacock