cancel
Showing results for 
Search instead for 
Did you mean: 

Which silicon revision code is actually in production for the STM32H7 family?

mhafn
Associate

Does anybody know which silicon revision code is actually in production for the STM32H7 family?

1 ACCEPTED SOLUTION

Accepted Solutions

​Looks like there are three revisions of this part: Y, X and V with V being the latest.

Application note AN5312 talks about the differences between them:

https://www.st.com/resource/en/application_note/dm00609692.pdf

I'm wondering how we can order a specific revision.

View solution in original post

8 REPLIES 8
Uwe Bonnes
Principal III

From the errate sheet I guess 0x2001

​Looks like there are three revisions of this part: Y, X and V with V being the latest.

Application note AN5312 talks about the differences between them:

https://www.st.com/resource/en/application_note/dm00609692.pdf

I'm wondering how we can order a specific revision.

There is also an older Z version.

>>I'm wondering how we can order a specific revision.

It will probably be difficult to get older parts as new silicon is available.

You'll want to qualify functionality of all that you use. Probably not going to be a huge issue as the key features will be additive and working.

Most of the stuff I've seen is Y, the X is about a year old.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Rev.V is out.

According to errata, there's no fixed erratum compared to rev.X.

Errata and RM mentions 'H742.

JW

https://www.st.com/en/microcontrollers-microprocessors/stm32h7-series.html

Now saying 480 MHz

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Which of course because of their silly off-line MCU selector program not auto-updating and hence still saying 400MHz, nobody (well me anyway) will know about.

Sigh.

The DS has two sets of electrical characteristics - one for rev.Y and one for rev.V; the latter having an extra VOS0 setting of the internal regulator enabling the 480MHz operation, It's subject to a somewhat limited Tj though, so it's sort of an "overclock", temperature to be watched closely in the application.

JW