cancel
Showing results for 
Search instead for 
Did you mean: 

Where to find - lowest Vcc value for mcu

oeliks
Senior

Hi, Can someone help me find the minimum voltage Vcc of stm32f103c8.

Lo​west voltage that will allow for maximum clocks frequency. And wont interfere with usb (pullups at data line to vcc).And adc.

2.4 V is minimum when using adc. But will it run at max clocks at that voltage?

1 ACCEPTED SOLUTION

Accepted Solutions
Piranha
Chief II

Datasheet sections 5.1.1 and 5.3.1 answers this perfectly.

View solution in original post

3 REPLIES 3
Piranha
Chief II

Datasheet sections 5.1.1 and 5.3.1 answers this perfectly.

oeliks
Senior

Ok, so min is 2,4V - 2.3.9 min vdda when using adc.

Thanks

Surely better parts, providing VDDUSB to keep drivers within specs.

People doing low voltage / low power typically using L0 or L4 at this point.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..