Skip to main content
csara.1
Associate
October 9, 2022
Question

Where is my problem to read ADC value (STM32F407VG)?

  • October 9, 2022
  • 0 replies
  • 515 views

Hello,

I want to read 8 bit ADC value from ADC2(PA1 pin) and use it to control a LED which is connected to DAC1(PA4 pin). I wrote a code(using registers) as below, however, I cannot read the ADC value(I tested it on STM Studio). Where is my problem? Thanks.

#include "stm32f4xx.h"

#include "stm32f4_discovery.h"

void ADC_Config();

void RCC_Config();

void GPIO_Config();

void DAC1_Config();

uint8_t c=0;

uint8_t adcread();

int main(void)

{

ADC_Config();

RCC_Config();

GPIO_Config();

DAC1_Config();

 while (1)

 {

c= adcread();

DAC->DHR8RD =c;

 }

}

void DAC1_Config(){

RCC->APB1ENR|= 0x20000000;

DAC->CR|= 0x00000001;

DAC->SWTRIGR=0;

DAC->DHR8R1|=0;

}

void ADC_Config(){

RCC->APB2ENR |=0x00000200;

ADC2->CR1|=0x02000000;

ADC2->CR2|=0x00000001;

ADC2->SMPR2|=0x00000018;

ADC->CCR|=0x00010000;

}

void RCC_Config(){

RCC->CR |= 0x00030000; // HSEON and HSEONRDY enable

while(!(RCC->CR & 0x00020000)); // HSEON Ready Flag wait

RCC->CR |= 0x00080000; // CSS Enable

RCC->PLLCFGR |= 0x00400000; // PLL e HSE seçtik

RCC->PLLCFGR |= 0x00000004; // PLL M = 4

RCC->PLLCFGR |= 0x00005A00; // Pll N = 168

RCC->PLLCFGR |= 0x00000000; // PLL p = 2

RCC->CFGR |= 0x00000000; // AHB Prescaler = 1

RCC->CFGR |= 0x00080000; // APB2 Prescaler = 2

RCC->CFGR |= 0x00001400; // APB1 Prescaler = 4

RCC->CIR |= 0x00800000; // CSS Flag clear

}

void GPIO_Config(){

RCC->AHB1ENR |= 0x00000001;

GPIOA->MODER |= 0x0000000C;

GPIOA->OSPEEDR|= 0x000000C;

}

uint8_t adcread(){

uint8_t value=0;

ADC2->CR2 =0x40000000;

while(!(ADC2->SR&0x00000002));

value=ADC2->DR;

return value;

}

void EVAL_AUDIO_TransferComplete_CallBack(uint32_t pBuffer, uint32_t Size){

 /* TODO, implement your code here */

 return;

}

uint16_t EVAL_AUDIO_GetSampleCallBack(void){

 /* TODO, implement your code here */

 return -1;

}

This topic has been closed for replies.