‎2021-07-02 12:00 PM
‎2021-07-02 01:21 PM
Take a clear, large and in-focus picture and attach.
Some of the earliest H7 perhaps 2017, the H745 2019Q1, perhaps late 2018
‎2021-07-02 04:33 PM
‎2021-07-02 07:30 PM
That is an STM32F407IGH6 perhaps 2009 / 2019, this is not an H745
‎2021-07-04 09:08 PM
Thank you very much
‎2021-07-07 11:10 PM
Hi,tesla:
I made mistake. please refer to the attached photo. I have the following questions.
2. When flashing M7 large code, segment[2] fails, but when flashing M7 smaller code (not using segment[2]), it works fine.
thank you very much.
‎2021-07-09 07:24 AM
Hi @forest xu​ ,
To identify the bootloader version, you need to refer to the section "Bootloader identification" in AN2606 STM32 microcontroller system memory boot mode.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
‎2021-07-16 10:42 AM
Thank you !