2017-06-26 6:39 AM
Hi,
STM32F446 user here. I'm routing RTC alarm output to PC13 and after an alarm I need to clear the output pin back to low state. I recall myself reading something about clearing RTC alarm output in a specific way but I can't find the source anymore.
#rtc #pc13 #alarmSolved! Go to Solution.
2017-06-28 5:06 AM
Found the answer.
'When the calendar reaches the alarm A pre-programmed value in the RTC_ALRMAR register (TC_ALRMBR register for alarm B), the alarm flag ALRAF bit (ALRBF bit), in the RTC_ISR register, is set to ‘1’. If the alarm A or alarm B flag is routed to the RTC_ALARM output (RTC_CR_OSEL[1:0] =�01� for alarm A, and RTC_CR_OSEL[1:0] =�10� for alarm B), this pin is set to high level or to low level, depending on the polarity selected. The output toggles when the selected alarm flag is cleared.'
2017-06-28 5:06 AM
Found the answer.
'When the calendar reaches the alarm A pre-programmed value in the RTC_ALRMAR register (TC_ALRMBR register for alarm B), the alarm flag ALRAF bit (ALRBF bit), in the RTC_ISR register, is set to ‘1’. If the alarm A or alarm B flag is routed to the RTC_ALARM output (RTC_CR_OSEL[1:0] =�01� for alarm A, and RTC_CR_OSEL[1:0] =�10� for alarm B), this pin is set to high level or to low level, depending on the polarity selected. The output toggles when the selected alarm flag is cleared.'