2021-01-28 02:58 AM
2021-01-28 03:35 AM
Having a title and the text in the body is good habit. Posting everything in the title is not.
Post a sharper image!
While F1 is cortexM3, F0 would be CortexM0. Code compiled for CortexM0 will run on M3, but peropheralsl are different, so probably it will not work! Look e.g. with findchips.com for that part.
2021-01-28 03:49 AM
"Posting everything in the title is not"
Indeed. But it doesn't help that the forum allows - even encourages - it.
:persevering_face: :tired_face: