Question
What is the maximum frequency that the ETR of a timer can support?
Hello.
I do not find in the datasheet (for example STM32F072) information that will allow me to conclude what the maximum clock frequency the timer (for example TIM1) hardware (via ETR) can support.
Can you help me?
I have knowledge of similar experiences with PIC18 and the timer can handle frequencies up to 100MHz ... but I do not find data in the STM32 datasheet that can substantiate this doubt.
Thank you.