2019-12-31 08:20 AM
Sorry for the dumb question, but I am rather new to this family of products.
I need to have two different possibility to exit a LP mode in different phases: in one case I can wake-up via the internal comparator, and this can be done even in STOP mode, no problem, but in another case I have to be awakened by an external device that is enabled setting one GP output high, so in this case I need to keep the status of that GP output even in the LP mode.
Can I do this in STOP mode, or what is the best alternative LP mode?
Thanks.
Solved! Go to Solution.
2020-01-16 08:02 AM
Hello,
Yes you can keep the state of the GPIO that you need, and put the rest in analog state in order to save power consumption.
Best Regards,
Mohamed Aymen.
2020-01-16 08:02 AM
Hello,
Yes you can keep the state of the GPIO that you need, and put the rest in analog state in order to save power consumption.
Best Regards,
Mohamed Aymen.