cancel
Showing results for 
Search instead for 
Did you mean: 

What is the GPIO state at standby mode with RTC?

ATahi.1
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
Mohamed Aymen HZAMI
ST Employee

Hello,

Yes all the unused Pins should be in analog state and you can keep the used Pins in the mode you have already configured.

Best Regards,

Mohamed Aymen.

View solution in original post

3 REPLIES 3
Mohamed Aymen HZAMI
ST Employee

Hello,

You need to put the GPIOs in analog state.

Best Regards,

Mohamed Aymen.

ATahi.1
Associate II

@Mohamed Aymen HZAMI​ You mean all un active pins should be in analog state? If I already put some pins in output high/low or Pull-up/ pull-down in idle mode, what is the state for those pins in standby mode? Are they going to have high impedance or would they preserve the orginal configurations in order to not have power leakage?

Mohamed Aymen HZAMI
ST Employee

Hello,

Yes all the unused Pins should be in analog state and you can keep the used Pins in the mode you have already configured.

Best Regards,

Mohamed Aymen.