2017-07-09 08:12 AM
STM32Cube_FW_L4_V1.8.1 returns 1.7.1
STM32Cube_FW_F7_V1.7.0 returns 1.2.1
STM32Cube_FW_F1_V1.4.0 returns 1.0.4
STM32Cube_FW_F4_V1.16.0 returns 1.7.1
So does this mean its all HAL 1. and the other numbers are implementation specific?
2017-07-10 01:42 AM
Hi
doe.john.016
,The
HAL_GetHalVersion function returns the HAL revision and not the
Cube firmware version.
Regards
Imen
2017-07-10 03:55 AM
This is why it's called abstraction. ;-)
(Sorry, I couldn't resist).
Jan