2021-08-30 02:03 PM
The STM32G030J6M6 is the SO8N device.
The Datasheet lists different functions upon reset for pins 4, 5, 8
Any help appreciated
2021-08-30 02:22 PM
The SWD pins (PA13/PA14) are initialized as such at reset. Others are initialized in high impedance input mode.
NRST is NRST, unless disabled in option bytes.
> The Datasheet lists different functions upon reset for pins 4, 5, 8
Where? I only see it call out PA13/PA14 (pins 7 and 8).