cancel
Showing results for 
Search instead for 
Did you mean: 

Using TCXO with STM32L0

JR2963
Senior II

Hello,

I would like to use TCXO (25 MHz) for timing STM32L071. It doesn't really work for me. When I put a scope probe behind C1, a signal can be seen in the picture. (some 27 Hz). Do you know what's wrong? The power supply for TCXO is 3.3

IMG_20240330_120959.jpgpcb.png

Please any idea? Thank you.

 

1 ACCEPTED SOLUTION

Accepted Solutions
5 REPLIES 5

HEY you are right!!  That's surprising! I'm currently observing a 25 MHz signal with about 2 Vpp between C and R.

Just can not see MCO outpu on PA8... Set in CubeMx..

 
 
 
 
 

@JR2963 wrote:

Just can not see MCO outpu on PA8... Set in CubeMx..


Read user manual to CubeMX (if exists), or set MCO by yourself without CubeMX... In LL API on STM32F0 it takes about three or four lines:

LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA); // Enable GPIOA clodk
LL_GPIO_SetPinMode(GPIOA,LL_GPIO_PIN_8,LL_GPIO_MODE_ALTERNATE); // Set PA8 to "alternate"
LL_GPIO_SetAFPin_8_15(GPIOA,LL_GPIO_PIN_8,LL_GPIO_AF_0); // select appropriate alternate function
LL_RCC_ConfigMCO(LL_RCC_MCO1SOURCE_SYSCLK,LL_RCC_MCO1_DIV_1); // select MCO source


By the way, what is purpose of C1 and R14 and how do you control DC voltage at PH0 input ?

Now the MCO output works. Thank you!

So you think C1 and R14 are not necessary and I can connect it directly? (I came from some STM32 wiring where I saw C and R.)

More than unnecessary. I think that its wrong.