Using PC_1 and PC_5 results in a faulty reading values, Why?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-08 6:53 AM
The question is regarding Nucleo-l476RG, I need to use 5 ADC, 12Bit.
No matter what I do. I cannot see that these pins are connected to anything else.
Why do I get a wrong reading on these GPIO?
Please notice that my board is new .. the MCU is not damaged.
I used the PB_1 for the same measurements and it works just fine. I have no idea why this happens.
I use mbed-os in my project .. I don't think it is mbed-os's fault either.
- Labels:
-
ADC
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-08 7:30 AM
Check solder-bridge options for PC1
If it is not hardware, then it is software. Proof the design using HAL, LL or register level code. Probe the pin-to-pin with a meter.
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
‎2019-05-08 10:20 PM
HW was OK.
And why should the mbed not work just for these two pins? I don't get that.
The value reads from these pins seems to be multiplied by factor > 1.5
The same software I used with PB_1 and it works just fine.
Don't know what could cause that.