2022-08-29 6:53 AM
I am using SPI1 as a Master full duplex , and checking in the Nucleo 429 zi
PA5 ------> SPI1_SCK
There is no clock , I using a scope and testing PA5 pin on the Nucleo 429 zi
I attach the code , its very short code
Here is the link to the pin description
2022-08-29 7:18 AM
Pull the schematic, CAD Resources Tab of product page.
Trace the wire from IC pin to header(s)
Watch for solder bridges and zero-ohm resistor options
Check GPIO clocks, Check GPIO register settings.
Check AF mux mapping. Check GPIO toggles manually
2022-08-29 7:35 AM
Thanks Tesla
I can see the SPI1_SCK , the clk amplitude is about 0.5 volt , that is the reason i didn't see on the scope
Now i have to figure out why i don't see the MOSI
Do you have any suggestions
2022-08-29 8:53 AM
> Do you have any suggestions
Yes, he had suggestions. Read his post again. Start with the first sentence, do what it suggests, and then proceed to next one.
JW
2022-08-30 4:42 AM
Thanks ,
I will do what you suggest
I test the program on some new Nucleo 429 zi that i bought from digikey ,
and in all of them it is the same result
I test the program it on SDI 1,2 and it is the same GPIO signals has 3 volt amplitude
Raz
2022-08-30 5:40 AM
Hi Tesla ,waclawek.jan
I did your recommended suggestions and they were OK , it was by multimeter and scope
---Still have a problem ----
Is it OK that SDI SCK amplitude is 0.5Volt ?
Still do not see using a scope any signals on the MOSI pin
Mention that the pins are not connected to another board and i only measure by a scope each SDI pin
Regards
Raz
2022-08-30 7:17 AM
Hi Tesla
After searching , I found this link in the internet
https://github.com/stm32duino/Arduino_Core_STM32/issues/1112
I think it will help me
What is your suggestions ?
Regards
Raz
2022-08-30 8:30 AM
Hi Tesla
I think i found the Mosi signal , Its not PA_5 it is in in PB_5
Why it is written in the figure (Pin description) above PA_5 ad PB_5 are SPI1_MOSI
What is the difference ?
Regards
Raz
2022-08-30 8:47 AM
Thanks for your help Tesla
the problem is solved